//======================================================================
// ASIX MCS7832/MCS7830 Windows 8.x Drivers Setup Program
// Revision History
//
// This document describes the major changes, additions and bug fixes made 
// to the program between released versions. 
//======================================================================

Note:
=====
Before run the setup program to install newer driver, please uninstall the older driver
that user installed before. User can check the list in "Control Panel" -> "Programs" ->
"Programs and Features". If there is a MCS783x (MCS7832/MCS7830) driver in the list, 
uninstall it before run the setup program.

Version 1.0.1.0 (2014-04-08)
1. This setup program includes the following MCS783x Windows 8.x 32-bit/64-bit drivers.
   MCS783x Windows 8.x 32-bit WHCK driver v1.16.1.0
   MCS783x Windows 8.x 64-bit WHCK driver v1.16.1.0
2. Changed to shorter driver installed folder names and update a new product code.

Version 1.0.0.0 (2013-01-21)
1. This setup program includes the following MCS783x Windows 8 32-bit/64-bit drivers.
   MCS783x Windows 8 32-bit WHCK driver v1.16.0.0
   MCS783x Windows 8 64-bit WHCK driver v1.16.0.0
2. Built the setup program by using InstallShield2010 Premier from this verison.